The screen brightness of your thermostat is at its maximum level when your are using it. When your thermostat is in standby mode, the screen brightness is, by default, automatically adjusted according to the ambient light. It is possible to change the screen brightness of your thermostat in the Home + Control App : go to settings, select "Manage my home", select the room in which the thermostat is installed, select the thermostat and select "Advanced", then you will be able to put the screen brightness always off or to set a customized level.
If you have already configured your installation via the Home + Control App, the number is available in the application settings: select "Manage my home",select the room in which the thermostat is installed and select the thermostat. You will find there the serial number.Otherwise, follow these steps to recover the serial number of your thermostat:1) Power off you thermostat directly in your electrical panel.2) Take a screwdriver and insert in the hole on the bottom side of the thermostat. Gently press to remove the front panel of your thermostat.3) On the back of it, you will find the serial number starting with 00:03:50
Even if I have more than one Classe 300EOS with Netatmo, just one will be the gateway. Together with this, at the launch just this same one will be allowed to manage through its touchscreen the automations. In a second release, it will be possible to use many touchscreens of Classe 300EOS with Netatmo of the same installation to manage automations.
The App Home + Security works also on tablet. When in landscape position, conceived for optimal video viewing, it is not possible to use answer/end call and open lock buttons. Just place the tablet again in vertical position to show and use the buttons.
For each account it is possible to associate more than one smartphone.However, it is recommended that each user logs with his/her own account on his/her smartphone.Tested up to 20 smartphones per account.
It is possible to disable the forwarding of doorphone calls to mobile devices by disabling WiFi on your Classe 100X.By this procedure your Classe 100Xwill be completely disconnected from Legrand cloud and the Home + Security App will be unusable from all devices both locally and remotely up to manual resetting of Wifi on Classe 100XTo desable the WiFi of your Classe 100X perform the following steps: press the configuration joystick on the right side of the video door entry unit to acces the main menu turn thejoystick downwards and press it later to access the "Settings" menu press the joystick again to disable the WiFi: the WiFi icon will appear with OFFTo enable again the WiFi of your Classe 100X perform the following steps: press the configuration joystick on the right side of the video door entry unit to acces the main menu turn the joystick downwards and press it later to access the "Settings" menu press the joystick again to re-enable the WiFi: the word "NO WI-FI" will appear for a few seconds and then the name of the WiFi network on which the Classe 100X was associated reappears